This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27220: Request for recommended PCB Land Pattern for the YZF package

Part Number: BQ27220

What is the recommended PCB Land Pattern for the YZF package?

I see that the solder balls are on a 0.5mm centered grid. and the solder ball size is 0.25/0.35mm (min/max).

Did I read the datasheet correctly on those dimensions?

Just wondering what the land pattern should be.

Thanks!

  • Hi Mark,

    You can access the EVM altium files to get answers to your question. Let me know if you do not have access to the repository and i will send you the files.

    thanks

    Onyx