This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir/Madam
We are using BQ25601 PMIC for one of our project ,
we are facing issue while using without battery (only input power is connected)
Output at SYS pin is 1.88 volt when we operated with USB 5V 500 ma Charger ,( battery is not connected). Maximum load is below 500ma
while probing on STAT Pin we are getting 50% duty cycled pulses, which means fault charge conditions. But we are unable to find out where the fault.
when we are connecting battery of 4.2v (Fully charged) same voltage is getting at SYS pin image of circuit is attaching for referring.
Requesting you to suggest solution for above issue.
Hi Mao,
Thanks for your reply.
As per your first point we suppose to get 3.6v to 4.2v at SYS pin without battery .But we are getting only 1.8v ,this is the issue we are facing.
Kindly suggest solution.
We assuming that there is no problem with our schematic. if there please comment that also.