Other Parts Discussed in Thread: PMP20795, , UCC256301
Hi,
Just started working with this IC and have had 5 pieces fail so far. The setup is based on PMP20795 reference design and i'm trying to power up from low voltage gradually rising to final voltage. Feeding 1.5V into BLK pin from external Dc source, applying 40Vac (rectified) to HV pin - Unit starts switching but on/off behaviour due to loss of Vcc & RVcc. Then i'm adding 12V to Vcc (through a diode, takes about 12mA) to get continuous swithcing - all ok so far. Gradually increasing Vac to about 120Vac - IC dies. Vcc and Rvcc seem to draw too much current. Layout is tight and grounding is good. Component values are similar to mentioned ref. design.
Any advice on the most likely causes for IC to fail like this?
Thanks,