This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a problem with LM3485 switching frequency. I made simulations in WEBENCH, in LTspice and everthing was ok - frequency was about 409 kHz. So I've designed custom board with LM3485 buck DC/DC converter 24 V - 5 V (max 2 A) I took parameters of components from my simulations (schematic form WEBENCH in attachments).
What I've got?:
Output voltage is 5 V, but switching frequency is about 4 MHz when I have Cff on PCB, and 1.3 MHz after I removed Cff! So temperature of transistor was very high (very poor efficeincy) when I reduced impedance of load and I must replaced PFET twice during tests.
I am attaching screens from my scope (without Cff and load was 430 Ohms) and schematic from WEBENCH (is the same on my PCB).
User,
Please label the scope shots. I'd like to be sure I know what I'm looking at.
Please also share the layout as well as the part numbers for the FET and diode.
Thanks,
-Sam
Oh I see the scope shots are just different time scales. Please send scope shots for a 2A load with and without CFF. Please also put VIN and VOUT on the other channels.
Pawel,
Thanks for sharing the schematic and layout.
I believe this is an issue with excessive FB ripple caused by the layout. The FB components (C15, R21, R22) connect to VOUT on a large plane far from the output capacitor. I believe this noise is triggering the 10mV hysteretic comparator at every transient causing an immediate toggle of the SW node. To test this I recommend scraping off a bit of solder mask near the connection point of the FB trace to FB plane and adding a 1uF ceramic cap (see below).