A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Aided by Webench, I designed a buck DC/DC converted based on the LM3485MM/NOPB
- Input DC 20 V - 25 V
- Output:12 V at 2.5 A
Once manufactured the DC/DC converted, it is not protected against short circuits.
Webench proposed
- Radj = 82.5kOhm
- Rsense = 20mOhm
Actually, I should decrease Radj downto 15kOhm in order to get the DC/DC protected against shortcircuit. This new value of Radj is coherent to the datasheet but it is not aligned to the Webench recommendation.
Please follow the recommendations stated in the datasheet. The datasheet will almost always be more reliable than WEBENCH because it is made so precisely to explain the details of the part. WEBENCH is better for system design and applications. We will look into this discrepancy. Thank you for bringing it to our attention.