This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI partner,
My customer use LM3485 for a buck application, basic case is input 24v, output is 12v/3A; the schematic and pcb as below
there are several question need to be consult.
1.why our datasheet typical application is different from our Webench power design schematic. if we adopt datasheet schematic, the circuit cant run normally and no output voltage, if refer to webench schematic, it is can output voltage.can you tell me the reason?
2. when we designed the schematic according to webench schematic, as above schematic. only the inductor is welded in one direction,the circuit is normal, in contrary, if we change the inductor welding direction, the LM3485 is very hot. the inductor is SDR1307-100ML,we also try other brand inductor such as MSS1210-473ME. can you tell me why, as i know ,the inductor don't have welding direction.
we also catch the PGATE pin (pin 7) waveform in these two case ,as below ,the first picture is normal waveform, the second is abnormal waveform ,please refer to.
look forward to your reply.
best regards
Cickey Xu