This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51275: What's the different with TPS51275 with TPS51225?

Part Number: TPS51275
Other Parts Discussed in Thread: TPS51225,

Hi Sir, 

I have some questions of TPS51275 and TPS51225.

1. May I know what's the biggest difference between TPS51225 and TPS51275?
    I only saw the Vin(min.) and duty cycle are different.

2. Why does it show TPS51275 can regulate 4 output and Iout(max) is 20A on the website?
    On the datasheet, the TPS51275 as same as TPS51225 only can regulate 2 output number and the gate driver ability or OCP parameter are the same.

3. Which device I could use?
    For 5V, Iout(max) = 16.82A 
    For 3.3V, Iout(max) = 14.71A