Other Parts Discussed in Thread: TPS92602-Q1
Hi, I am a student and i want to start my project to drive high power LED.
My LED specifications are:
Size: 34*34*1.0mm
Power: 100W
Current: 2A
Voltage: 70-75V
Peak Irradiance: 8W/cm2
Viewing Angle: 60 degree
Chips Arrays: 40 chips, 20 in Series 2 in Parallel
Can you please suggest me that TPS92602-Q1 is a good choice for my LED ? As far as i searched it out i didn't find any other than this which is almost completing the requirement of my LED.