Other Parts Discussed in Thread: TPS61169
Hi team,
Can I connect VOUT_A to not only LEDA1~6 but also LEDB1~6? (only use one boost component like L and diode)
Or do you have other suggestion to fulfill below spec? if single channel can't do that, just let me know do we have other product which can support total 12Vout/500mA output.
Thanks
Vin range: battery power (3.6~4.4V)
12V output WLED backlight
Single channel to support max 500mA output
I2C is needed
AEC-Q100 is not needed