Other Parts Discussed in Thread: LM2594
Hi Texas Instruments,
I am designing a step-down power management circuit for 48V that should output 5V using LM2594HV.
I am having a problem selecting the input capacitor for the circuit, the datasheet suggests to use a Tantalum capacitor or Aluminium electrolytic with a voltage rating of 1.25 times the input voltage.
The input of 48V doesn't really make tantalum a choice, since all Tantalum caps with 60V (40*1.25=60) costs 50 EUR or more, and it is not in my budget for this board.
The Aluminium electrolytic caps I am finding with 60V rating seem to have quite large footprints (in the range of 3-6 times the size of the LM2594HV footprint), and this ideally does not work on my intended layout either.
When looking at the layout example in the datasheet it is seems that the footprint for the capacitor you have chosen is quite small (in the same size at LM2594). Did you by any chance use a ceramic capacitor here? If so, why have you done that when you recommend tantalum? What would I be trading off if I choose to use a Ceramic capacitor instead? (Ceramics can easily be found with 100V rating with a small footprint).
What would you suggest me to use if I want to keep to about the same size as the layout example?
Thanks in advance!