This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在LM5146-Q1 SPEC中寫到
若使用RDSON,LM5416 IC內部裡面有個ILIM會有一個200uA給RDS(ON)
若使用RSENSE電阻,5416 IC內部裡面有個ILIM會有一個100uA給RSENSE
在PG.40的範例去計算RILIM的值,我去計算當Vin=85V的ΔI 及Vin=14V的ΔI, 再去算流過RDSON上的跨壓, 利用公式算出RILIM ,但用公式去計算與範例的RILIM=619 Ohm差異很大,以範例電路圖中的RILIM=619 Ohm * 200uA=0.1238V, 以0.1238V+(-9.8944A)*10 m Ohm=0.12281V,電路一開機就進入OCP保護了,想問這邊的RILIM=619 Ohm怎麼算的
Hi Oscar,
As Wei-Hao mentioned, this question is addressed at the link he provided. If it's okay, I'll go ahead and close out this thread.
Regards,
Tim