This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer has an application question regarding DEMB function of the LM5146-Q1 when external driver is used. My customer wishes to use external driver with LM5146 due to the SW & BST rating is not enough for their application.
In our previous experience, when external driver is used the SW pin tends to be grounded, however the DEMB function will not work because SW detects the zero-crossing when hitting the zero current. But now it is grounded which cannot detect the zero crossing anymore
Would you please suggest a circuit to achieve DEMB function while external driver is used? They tends to use UCC27712 for the external driver.
Thank you!
Best Regards,
Wei-Hao
Hi Wei-Hao,
As you know, the LM5146-Q1 has integrated gate drivers. It is not designed to operate with external gate drivers. If SW is grounded, the current information for zero-cross detection is lost - this is required for pre-bias startup, diode emulation mode operation, as well as adaptive deadtime optimization for MOSFET switching.
Maybe we can recommend another part. What are the input and output specs for this application?
Regards,
Tim
Hi Tim,
No long no see, hope all is well. I will convince my customer not to use the external driver. They have some other questions wants to clarify:
1. The VILIM-TH spec has very large range, is this the offset of the ILIM comparator or the ILIM threshold? if yes, the OCP range will varies a lot. Could you please check the OCP accuracy?
2. How to select the proper value for Rs and RLIM to set the OCP. The equation 6 provide how to calculate RLIM, but it did not include how to select the appropriate Rshunt. May I know how should customer design the Rshunt first?
3. Figure shown on page 16 (function block diagram) and Figure 34 on page has swapped input pins of the internal ILIM comparator, can you please check which is correct?
Thanks a lot.
Best Regards,
Wei-Hao
Hi Tim,
Thanks for your suggestion, but the voltage rating for LM5143-Q1 is enough for my customer's application.
Also they have two follow-up questions regarding LM5146-Q1.
1. The design example (9.2.2 Design 2 – High Density, 12-V, 8-A Rail From 48-V Automotive Battery Power & ) that is in the datasheet has relative large Rlim setting than expected. Based on my customer's calculation the RLIM should be around 300~400ohms, but the value shown in the design is 619ohm. Could you please check how to derive this 619ohm resistor?
Here's how my customer calculate the expected RLIM value, is this correct?'
2. How to achieve CC mode on LM5146? As we know pulling the COMP pin might have some problems. Would you suggest a reference circuit for CC/CV with LM5146?
Thanks lot Tim, really appreciate you support.
Best Regards,
Wei-Hao