This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello...
I recently found the cool BQ24195 IC, but it seems to be designed to charge a single-cell Li-Po battery, take in USB power, and power a 5V load. Makes sense.
Is there a version of the BQ24195 family of ICs, or a very similar IC, that charges a single-cell Li-Po battery, takes in USB power, but provides a 3.3V output for the load?
Or do I need to simply use an LDO or buck IC to go from the 5V down to 3.3V?
Thank you!