This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
My customers are considering TPS566637.
Therefore, the following documents are required.
Does anyone have it?
・weight
・MSL
・Reflow condition
Best regards,
Yurie
Hi Yurie,
Please check the information below:
MSL/Reflow Ratings: LEVEL2-260CG
Total Device Mass(mg): 19.5793
Also, an application note introducing MSL Ratings and Reflow Profiles can be found by the link: http://www.ti.com/lit/an/spraby1/spraby1.pdf
Thanks.
Best Regards,
Bruce
Hello,Bruce
Please let me ask you a question.
Is it possible to rework using a soldering iron?
I think it seems impossible as long as I look at the package.
If possible, can you also tell me about the soldering peak heating temperature (° C) and the soldering peak heating time (sec)?
Best regards,
Yurie
Yurie,
It has potential risk if you rework with soldering iron because of the MSL level 2 limitation. But the risk is low if you only rework several boards.