Other Parts Discussed in Thread: BQ25703A, BQ24773, BQ25890
I could easily find PMIC IC's for lithium battery powered devices with good application information (I need to get it to work quickly) for small currents and USB charging.
I want to know if you can advice on an IC that can handle charging multiple Lithium cells (3 or 4 series, or all parallel), with a managed system output current between 5 to 10A, and that can also switch from the battery to the charger, something that I guess would be used in a standard Laptop power management system.
So far it looks like I will have to put together a few IC's, and use more components than I have space for.
Thanks in advance