This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM25119: LM25119 Output voltage Low

Part Number: LM25119

Tool/software: WEBENCH® Design Tools

based on webench design, my Vin=28V, using LM25119 as an interleave/single output, per recommended schematic, Vout is expected to be 24V, Iout=19A (9.5A each channel).  However, upon power up Vout=1.2V.  With selected Rt, the switching frequency is about 172Khz. I can see this switching waveform on scope.

Can anyone points me to where to start troubling shooting?