Other Parts Discussed in Thread: LMZ31710
Hi, team.
Does it break if the output voltage of the LMZ31520 is 4.1V?
It is good not to break even if the voltage accuracy and various characteristics worsen.
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Since the switching power supply board and the sensor board are separated as shown in the block diagram, the power is supplied by the cable.
Considering the voltage drop due to the cable, it is set to 4.1V.
Although it is somewhat special usage, DC / DC can not be placed on the sensor board side, so it has such a configuration.
Although the number increases, we propose parallel use of LMZ31710.
Thanks,