I am using multiple TPS549B22 in my design. I want to control the EN_UVLO through a controller. Below are the operating conditions of TPS549B22.
Vin = 12VDC
Vout1 = 2.3V;
Vout2 = 1.55V;
Vout3 = 3.7V;
My controller output is 3.3V CMOS. This is connected to EN_UVLO of TPS549B22. Will this work or do I need higher voltage levels?