Dear TI,
I am looking for a Buck/Boost Regulator that able to output 5V and 1A. The source of the power is from 2 cell LiPo 7.4V. The battery fully charged Voltage is 8.4V and start to discharge to cut-off Voltage of approximately 3V. So I need a regulator that able to output 5V and 1A for the entire discharge.
WeBench recommended TPS63070RNMR, and below is the circuit from WeBench. I have looked at the datasheet and seems good to me, but need a second opinion.
Questions are,
1. Is this chip able to support LiPo and output 5V and 1A?
2. Is this below circuit is good to go for initial stage?
BRgds
Manimaran