Other Parts Discussed in Thread: BQ25606
We implement BQ24266 at our new product and unfortunately the charger is not working
The issue describes below:
when the USB2 (in fact I am using Power Source 5VDC @ 3A ) and the battery 1 cell Li-ion 3.7 Installed I can’t see current consumption
The Monitored values are:
- TS – 2.65V @ VDRV= 5V
- ISET – configured to 400ohm
- USB1- Low, USB2&USB3 – High
- The Input voltage to the charger 5v
Pls. advice...