This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825A: UC1825A

Part Number: UC1825A

Hi TI Support,

I am looking for more detail information regarding the UC1825A (5962-8768012V2A) Error Amplifier parameters variation (Vio, Iio, Ibias).

1) Input offset voltage is listed as 2mV nominal and 10mV max. Is this variation due to both Temperature and Radiation ? If TA range is 125C, Can I calculate Vio variation using linear approach for lower temperature ?

2) Similar question in item 1 for Input bias current and Input offset current

3) Are Vio, Iio, Ibias varies as random or uni-direction ? Could you provide some test results due to temperature and radiation.

Please send information to my email address.

Thank you for your support

Best Regards,

Jason