This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65631W: TPS65631W turns off immediately

Part Number: TPS65631W

I'm using the TPS65631W in a design with AMOLED display.  The 4.6V comes up and then immediately turns off in about 100us.  I don't think it is the Short-Circuit During Start-up since it doesn't kick-in until 10ms.  With no load (AMOLED), both voltages come up fine (4.6 and the programmed -2.4). The display consumes about 20mA during normal  operation (NON-Startup).  I have perform several tests with the displays and I believe they are operational.

I'm looking for any advice on how I should proceed.