Hello everyone,
I am using the UCC3808 controller in a Push-Pull Topology. As the duty cycle at steady state would be greater than 50% it is almost imperative the use of slope compensation. The circuitry that I am using to achieve that goal is shown next:
According to the datasheet of the 3800 (not the 3808) the timing resistor Rt could be broken up into two series resistors to bias up the NPN follower.
I would like to know if you consider that mandatory to the 3808 case. The voltage at the base should be around 1V, is not it?
(Page 23, http://www.ti.com/lit/ds/symlink/ucc3800.pdf )
Thank you for reading.
Best regards.
David.