A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ77PL157A4225: works with DEXERIALS SFK-4030 fuse?
Hi Vincenzo,
The bq77PL157 is designed to drive a low side FET as a protection element, that is the FET is on during normal conditions and turned off when there is an OV fault. So it will not control the SFK series fuse directly. A circuit would be needed to invert the OUT pin signal to turn on the fuse heater when the fault occurred.