Dear All,
one of my customer is using BQ77PL157A4225 and they are facing following issue, kindly need help to resolve the same.
In this one they are using the 4 series CELL'S Model.as per the drawing mentioned from the Datasheet. so in this they are facing one Problem and they are charging this battery management system through solar panel or Power supply and with that higher cutoff happen to batteries at 16.9V( any one cell reaches to 4.225 as per mentioned in datasheet 4X4.225 ) and after higher cutoff happens they are unable to identify where is reconnection point for charging by changing the CD Pin Capacitor values in the system as per data sheet and in this one they have observed one point that when it was in reconnection voltage drops below 15.2V to 15.4V with load or without load on the battery irrespective of the CD capacitor value its happening can you please suggest me the solution for this.because theywant to set the reconnection value to 16.2V.
Aravind.