This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

L293: Marking

Part Number: L293

Hi,
where can obtain informations about valid marking of the chip L293NE 75CE71M ?
The board is assembled externally and I supect a countrefeit because about 3% of mounted chips are not working and the logo and fonts are differents from the past.
The main defect is like a short between one (or more) inputs and 0V or the power supply.
Replacing the driver make the board working good, so others parts and pcb are ok.
Our standard production requires about 900 drivers/month and we don't have never see this problem.
Thanks