Hi,
I have a question about formula : ICINnorm(RMS)= Sqrt [(D-m/n) x ((1+m)/n -D)]
Is there phase limitation here? I assume the ICINnorm(RMS) will decrease when the phase count is increasing.
Below is my calculation:
D=0.275 (3.3V/12V)
n=2 ; m=0 ; ICINnorm(RMS)=0.2478
n=3 ; m=0 ; ICINnorm(RMS)=0.12665 (decrease)
n=4 ; m=1 ; ICINnorm(RMS)=0.075 (decrease)
n=5 ; m=1 ; ICINnorm(RMS)=0.0968 (*increase)
n=6 ; m=1 ; ICINnorm(RMS)=0.0794 (decrease)
n=7 ; m=1 ; ICINnorm(RMS)=0.0376 (decrease)
n=8 ; m=2 ; ICINnorm(RMS)=0.05 (*increase)