This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ21040: Cold this modules be placed in parallel to achieve more charging current than 1A?

Part Number: BQ21040

The charging current of 1A is not sufficient for my application. Could I use two[three] modules of a such type connected in parallel?

  • Hello
    Sorry but the BQ21040 cannot be parallel for higher charging current.
    For charging current in the 2A to 3A range a switching charger would be a better option.