Other Parts Discussed in Thread: BQ24160, BQ24133, TPS2121, TPS2120, TUSB320, BQ25601D, BQ25606, TUSB422, TUSB321, BQ25890
Team,
We are considering using one of the bq2416xx devices as those are dual input chargers with power path (that's what we need, the supplies are 5VDC and 5V USB).
Can you help to understand if the below system functions can be met?
- When 5VDC is present, 5V USB is present, Battery is fully charged -> system runs from 5VDC
- When 5VDC is present, 5V USB is present, Battery is NOT fully charged -> the battery must recharge but the system runs from 5VDC
- When 5VDC is NOT present, 5V USB is present, Battery is fully charged -> system runs from 5V USB
- When 5VDC is NOT present, 5V USB is present, Battery is NOT fully charged -> the battery must recharge but the system runs from 5V USB
- When 5VDC is NOT present, 5V USB is NOT present -> system runs from 3.5V to 3.7V Battery voltage.
Additionally, we are going to have USB type-C (only USB Type-C 5V 3A, not PD) - is that fine with bq2416xx?
Thanks for your help,
TI Customer