This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548D21: Request the Design Review.

Part Number: TPS548D21

hello

Can you Review the schematic for below specifications?

VIN : 4.8 ~ 5.8V

Output Voltage : 0.85V (+- 0.025V)

Output Current : 25A ~ 30A

OP Temperature : -40 ~ 80℃

Regards.

DTU_190226_TPS548D21RVFR.pdf