Hi to everybody,
in a new project design we've introduced TI's LMZ14203H in order to provide a regulated 24V from a 34Vdc input to a load: no problems at all at light load, while we are experiencing bad regulation at full load.
We've followed step by step the layout proposed by Texas.
The first strange behaviour is related to the switching frequency: instead of being 370KHz, it's actually 180KHz, and it does not vary by changing (halving) the resistance value on Ron.
This could be to some extent related to the main problem, that is: while at light load (Rload > 20ohm) the output is stable at 24Vdc and pin 6 voltage (FB) is 0.8V, at heavy load (Rload < 15R) the output voltage goes down to 22V and pin 6 voltage is 0.75V (the regulation is lost).
This is strange, since the IC should give full regulation down to Rload=8ohm...
Any suggestion?
I thank you in advance!
samuele