This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3825A: Control loop circuit doesn't work

Part Number: UC3825A
Other Parts Discussed in Thread: UC3825

Dear

I used UC3825DW to design a full-bridge power supply ,and the load is a 470Khz amplifer. 

when the amplifer works on 70Ws and 100 ohm status, the UC3825 didn't work normally. it's supposed to output 70Volts, but it outputs 100Volts.

And then i used UC3825ADW, there are some improved, but still not work normally when amplifier output power higher than 100W.

BTW, what's the defference between UC3825ADW and UC3823ADW?

I guessed there are some interference due to large pulse current.

could you give me some suggestion?