This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please help check the Power IC and recommend the blank

Other Parts Discussed in Thread: TPS63700, TPS63710, LMR70503

Hi Engineer,

Can you help check the Power IC and recommend the blank?

We need the automation level, great performance and the great cost.

I don't know how to find the Negative high voltage supply, If you can teach me, it will be so good.

Thanks a lot.

  • Hello Elsa,
    A very interesting design.

    Consider the TPS63700 for the 5V to -3V@0.1A
    The TPS63710 is a synchronous converter that would provide higher efficiency.

    For your +12V to -70V, it appears you want it variable from -70V to -300V @ 5mA.
    Please verify.
    This output may be difficult without a transformer, direct duty cycle for +12 to -300 will be an extreme duty cycle.
    A flyback design may be more appropriate.
  • Hello Elsa,

    For 5.5V to -3V, LMR70503 would be the smallest solution we have available as far as I know. The device is WCSP, sometimes customer do not like this package.

    For the negative converter, a flyback design is a possibility. Please have a look at this design: