Hi,
We are working with inverter designing for motor drive application..
Our preferred IGBT is SKM100GB12T4. Its gate capacitance Qc = 565nC at Vge=-8V to 15V.
switching frequency : 20kHz, Gate resistance Rg = 10 Ohm, . Internal gate resistance : 7.5 Ohm
Average gate current : 11.3mA and peak gate current is 1.3714A
Power required per channel is 271.19mW.
1. Shall we use ISO5852S to drive this IGBT or do we required external gate current buffer circuit?
2. How to calculate the values for Rg (on) and Rg (off) in ISO5852S ?
Kindly confirm the details to proceed further.
Thanks & regards,
Rajasekaran