Hi,
we have the same issue as David Boyle1 ("TPS54319 failures"): a conducting path between PH (pins 10, 11,12) and GND (pins 3, 4). We have it on 2 out of 5 prototype boards (yet). On one board, there is a 1 ohm path from the beginning, on a second board, there has develodep a 3 ohms path after some 20 power cycles. It is very unlikely a thermal problem as we have followed the TI recommendations on thermal vias and we draw only some 0.5 amps typically (max 1 amp). The parts have the lot number C6Q7. Unfortunately, David's post has been locked. The part is powered with 5V from another TI buck converter (working fine) and outputs 3.3V to another buck converter and to a Raspberry Pi.
Can TI please tell me
- whether there is a known issue with the above-mentioned lot?
- special schematic or layout considerations necessary to avoid this issue beyond the information provided in the data sheet?
Best regards,
Christian