This question is related to another question on this forum. Unfortunately, the answer to that problem was via a private email so I cannot see the answer. We have a design that has failing TPS40200HT parts. The design is resetting due to an over-current condition but only a nominal current is being used from the design at the time (1/2 the designed max current). We have noticed on the failing parts when the input voltage is varies from 28V to 32V the voltage on the soft start pin will change by ~150 mv (around 8.3V). When the part is replaced by a new TPS40200HT on the same board, there is no over-current shutdown and the voltage on the soft start pins if rock solid, not moving at all when the input is varied. Additionally, it seems like the failing boards' reset due to false over-current conditions much more frequently when the input voltage is 32V as compared to 28V. What condition is causing these parts to fail? According to the data sheet, this part can handle up to 52V input.
The original question on this forum was posted by Stephen Senn and the title was "Soft Start Pin steady state at 15V insetand of 8V". If the reply had been made public, my question would not be necessary! However, it seems like this part has a problem as two different designs are seeing very similar problems.