Other Parts Discussed in Thread: LM5141-Q1
Hi,
My customer will use LM5141-Q1.
My customers will buy TI's EVM and plan to do a test before designing.
The specifications are below.
Please tell me the changes in EVM to meet the following specifications.
(specification)
VIN : 16V(min), 24V or 48V(typ), 60V(max)
VOUT : 12V
IOUT : 0.1A(typ), 3A(max)
Operating frequency : 2MHz
Operating mode : FPWM
Also, the input filter is not used because the substrate size is small.
Also, I want to reduce the output capacitor as much as possible. Therefore, please tell me the minimum required capacity value.