Other Parts Discussed in Thread: TPS61196, TPS61165, TPS61181, LM36923H, LM3697
Hi
I would like to design a LED driver circuit as attached.
Please help to recommend TI LED driver solution.
Thanks!
Sincerely,
Chin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sean,
My design is for RGB individual LED string (see attached).
It means that the Vf are different.
Blue total Vf = 2.5 x 10 = 25V
Green total Vf =2.4 x 10 = 24V
Red total Vf = 1.6 x 10 =16 V
TPS66196 still suitable for this kind of design (different Vf connect to Vo together)?
Thanks!
Chin
Hi Sean,
Okay.
So if our RGB LED part internal architecture is connection anode together (see attached) and we connect it as LED string in the circuit, it means I cannot find suitable TI solution for the design? Is it correct ?
Thanks!
Chin
Hi Sean,
Okay , if our design igore independ control each channel output current , please provide a suitable TI solution to me.
See attached of our LED design, please note the different VF of LED RGB string.
Or we can use TPS61181 dor the design?
Thanks!
Chin