Hello,
We are using a BQ24064 with power being supplied to the device from a USB source which provides 5V +/- 5% = 4.75-5.25V. A key parameter for our design is the dropout voltage, as we also require additional protection components in the power supply path. We are using a charge current of 300mA, so would like to know the maximum dropout voltage at this current.
The datasheet provides two dropout voltage parameters: V(do) MAX = 750mV @1A and Figure 12, a graph showing variation of dropout voltage versus temperature. . Figure 12 could be useful to us as it shows the dropout voltage over temperature varying between 0.25V and 0.375V but doesn't state what charge current the graph is based on.
Could you provide any additional information for the dropout voltage at 300mA.
Thanks - Derek