Other Parts Discussed in Thread: TPS2114A, TPS2115
Hi All,
I'm looking to use a TPS2114A or TPS2115A to switch two voltage rails to some level translators, to allow me to control the levels. I need to switch 1.8V and 3.3V, which is covered by the TPS2115A's range. Per the datasheet, its all right to have an input of down to 1.5V, so long as the other Vin > 2.8V.
My concern is that due to our power sequence, the 1.8V will come up before 3.3V. Since the device will not be fully on, what will be the effects? Will the device just remain inactive, or do I run the risk of burning the input? My first solution to this is to FET switch, connected the 1.8V to the TPS2115 and controlled by 3.3V. Its a little bit of a roundabout solution, but now the 1.8V input will only be supplied while the 3.3V is active.
Thanks,
Rich