Hi all,
We are facing some thermal issues with a prototype of 40W LED driver based on LM3404HV (SOIC8).We are trying to drive a 38V 1A COB LED from an integrated 52V Flyback SMPS.The Flyback SMPS and LED driver is on a same PCB inside a plastic enclosure.Its working fine as open frame but when the enclosure is closed,working for a few hours the LED starts to blink.We also tried separating the SMPS part but it doesn't helped.We now doubt both the frequencies,switching and dimming.Please help !
VIN - 52 V
Vout - 38V
Iout - 950mA
Rcs - 0.2 ohm
Fsw - 250Khz
Fdim - 500hz (3.3V)
Ron - 1meg
Diode - MBRS4201T3G (SMC)
Inductor - 100uh 1.5A 10x15 Drum
Thanks and Regards.