Part Number: BQ76200
Hello, I'm using the BQ76200 to drive the bidirectional switch composed by two N-FET (Q1 and Q2) for the high-side protection of a battery pack.
My idea is to keep the two protection FETs always on in normal mode and turn off Q1 to inhibit battery charge and turn off Q2 to inhibit battery discharge.
Consider now the case where both FETs are on and I am discharging the battery.
My question is: how the discharging current overcomes the CHG FET Q1? Does it flows through Q1 body diode or it flows in the Q1 channel from source to drain?
I know that an N-channel FET is designed to conduct current from drain to source but I'm asking my-self if it is a bidirectional device able also to conduct current from source to drain (when it is on) bypassing the body diode.
This is an important aspect in my design because if the discharge current flows only through Q1 body diode I have to choose a protection FET with a body diode able to conduct a large amount of current!