Other Parts Discussed in Thread: LM3409, TPS92515
We found that the frequency of PDIM signal need to higher than 10khz to avoid the stripes . 20Khz will be better.
So i decide to use the ADJ pin to adjust the current instead of PDIM. I plan to connect the ADJ pin to MCU's DAC pin and use the PDIM as a ENABLE/DISABLE singal. Is there any risks to this solution?
Application scenarios: Two green led in series, 1A current, 3~4V each led. adjustable to the lightness.
Or could you help me to introduce another suitable driver IC to me?