This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28810: Connection doubts

Part Number: UCC28810
Other Parts Discussed in Thread: TL431, PMP

Dear Sir / Madam,

                                I am  new to power electronics, currently I am also doing the same circuit PFC + Flyback using UCC28810, I have some queries regarding the circuit connection,

1. There are two VDD tags ( next to C7 and R25 ) in the circuit, do i need to connect each other?

2. Like wise, on the transformer secondary side there also 2 VDC tags ( Next to R100 and D11 ), do I need to connect that also?

3. Subject to availability I have used 1N4148 instead of MMSD914 and 1N4007 instead of USK1K -13, I would like to know is it fine to use these alternatives in this circuit ?

I would be very grateful if some could help me with requested information

Reference Design ( page 1 ) : www.ti.com/.../slur512.pdf

 

Thanks in Advance

 

Kind Regards

George Thomas