This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25119: Consultation on LM25119 Use Problems

Part Number: LM25119

Hi,

The LM25119 application encountered the following problems in the 1200W laser power supply project:
Product information:
Input voltage 80-130V, output constant current maximum 20A, output voltage maximum 62V.
Laser driver: product constant current output, customer given analog quantity, adjust product output current.
Operating mode: Switch constant current, customer external given analog, dimming.

Solution: Using non-isolated staggered BUCK

Circuit as below:

Need TI's members help.

thanks.