Other Parts Discussed in Thread: LM5010
Hello,
I am after LM5010A-Q0, which is the same part but has higher temperature ranges.
Operating conditions are:
Input voltage: 24-60 V
Nominal Voltage: 48 V
Output voltage: 12 V
Output current: 0.6-0.7 A
Switching frequency between 171 - 200 kHz
Would this component withstand 120 deg C ambient temperature continuously for 7000 hours and among this time the temperature can rise for random duration up to 140 deg C, but total 140 deg C is going to be 120 hours?