This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2022A: SDQ pin question

Part Number: BQ2022A

Dear Sir.

As shown in the figure: The SDQ pin in the line has a 100R resistor. Please help confirm the following problem.

1. What is the specification of the resistance value range (minimum and maximum values) that the resistor R1 matches with the chip?

2. Can I replace it with other resistance values? For example, is it possible to directly connect 220R or 300R or not?

3. What is the impact of the resistance on the chip? The bigger the resistance are better or the smaller are better?