A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi user,
Can you give me more information about the application you are using BQ24610 for? Are you just using BQ24610 to charge a device at the output of the power stage of BQ24610, and you do not need powerpath, input-reverse blocking FET? If so you can take a look at the first page of the FAQ post which shows a simplified non-powerpath schematic for BQ24610