This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25119: LM25119: transient load issue

Part Number: LM25119

Dear Sir,

As below transient load waveform(output current 5A to 0A transient), output voltage overshoot too high over 200mV, 

Vin=20V ~ 36V,  Vo=12V/34A, circuit design interleaved mode(refer datasheet page 32 circuit)

DEM pin= floating(would improve light load efficiency)

RT=22Kohm(Fosc=220KHz); Output chock(L1= L2)=3.3uF, 

RAMP(R14+ C20) =73.2Kohm + 820pF ;  COPM1(R7 + C17 +C16)= 49K + 682pF + 100pF

Does L1=L2=3.3uF to low? 6.8uF is OK ?

Please you kindly review & provide suggestion(how to improve transient over-shoot)..

Thanks!

Steven