This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25119: LM25119: DEMB

Part Number: LM25119
Other Parts Discussed in Thread: PMP20021, PMP9700

Dear Sir,

DEMB(PIN17): floating is enable diode emulation mode and low side MOSFET latch-off. right ?

-> that mean LM25119 into  like as non-sync. Buck converter during output light load.

My customer try modify EVM make a 2phase output, output load transient  H -> L(5A ->0A) as previously waveform SW have stop condition(make have overshoot issue).

But when we put DEMB connect to VCC1 output transient waveform(SW) didn't have stop & output voltage transient waveform OK. It is correct behavior?

I saw TI design PMP20021/ PMP9700 the DEMB is connect to VCC.

Thanks!

Steven